Issue:
What are the voltages codes required to order a pilot light modification for the 2510 M Manual Starters?
Product Line:
NEMA Manual Starters and Switches
Environment:
Class 2510Type M Manual Starters
Resolution:
Include voltage code along with Form P11.
For example; red pilot light for 120 volts for the 2510MBG1 would be ordered as 2510MBG1V02P11. Available voltage codes are as follows:
110vac - 120vac = V02
208vac - 240vac = V03
440vac - 600vac = V06
What are the voltages codes required to order a pilot light modification for the 2510 M Manual Starters?
Product Line:
NEMA Manual Starters and Switches
Environment:
Class 2510Type M Manual Starters
Resolution:
Include voltage code along with Form P11.
For example; red pilot light for 120 volts for the 2510MBG1 would be ordered as 2510MBG1V02P11. Available voltage codes are as follows:
110vac - 120vac = V02
208vac - 240vac = V03
440vac - 600vac = V06