{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are the NEMA 4/4X/5 stainless steel, NEMA 12/3R, or NEMA 12K safety switches provided with a hub for conduit entry?
Issue:
Does Square D provides hub for conduit entry in NEMA Type 4/4X/5 stainless steel, NEMA Type 12/3R, or NEMA Type 12K safety switches

Product Line:
Safety Switches

Resolution:
No, watertight hubs should be ordered separately for field installation.
Type H hubs would be recommended for the NEMA 12/3R or NEMA 12K switches. Type H-CP hubs would be recommended for the NEMA 4/4X/5 stainless steel switches.
Field cut openings are required on the NEMA 4/4X/5 (suffix DS or SS) and NEMA 12/3R (suffix AWK) since no knockouts are provided on these switches.
The NEMA 12K (suffix A) switches are provided with knockouts.

Schneider Electric Canada