{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do you determine to use edgewise aor flatwise hangers when mounting I-Line busway?
Issue:
Selection of hanger types

Product Line:
I-Line Busway.

Environment:
Products sold in North America

Resolution:
Flatwise hangers hold the bus so that the bus bars are oriented with the flat side up and down. Edgewise hangers hold the bus so that the edges of the bus bars are oriented up and down. In the flatwise position, the plug-in units would mount on the sides of busway, not the top and bottom.

hangers

Schneider Electric Canada