{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
If you manually push the test button on a solid state overload relay, should it stop the motor?
Issue:
Describe what can happen if you click the test button in an overload relay

Product Line:
NEMA Type 9065 Overload Relays

Environment:
NEMA Contactors and Starters

Resolution:
Yes. If the unit does not trip, it is wired incorrectly or is not functioning correctly.


Schneider Electric Canada