{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the AL800M23K lug kit data for Powerpact M, P and NS630b-NS800 breakers?
Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
Conductor: Al/Cu
Lugs per kit: 3
Construction: Individually-mounted and I-LINE circuit breakers.
Tool required: Screwdriver, POZIDRIV #2 or #3, or slotted. Socket Wrench, 7mm hex (for wire binding screw). Torque Wrench, 5/16 in. or 8mm.
Conductors: 3
Size: 3/0 - 500 kcmil
Strip length: 1 in.
Wire binding screw torque: 442.5 lb-in
Lug mounting screw torque: 190 lb-in

Schneider Electric Canada