{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the EZM Metering devices have Series Short Circuit Current Ratings(SCCR) with down stream panels (QO or Homeline load centers)?
Issue:
Product design features

Product Line:
EZM Metering

Environment:
Series Short Circuit Current Ratings(SCCR)

Cause:
Application

Resolution:
Yes, The EZM metering equipment does have 3-tier series SCCR with downstream QO and Homeline Load centers. Please refer to the latest Square D Digest for details of the EZM series ratings and the publication titled "Square D Load Center Short-Circuit Current Ratings" document #4100DB0301 for the 3-tier SCCRs (See bulletin attached below)

Also, refer to the 3_Tier SCCR label that is applied to Every QO and Homeline Load Center. This label will be on the cover for the NEMA 1(indoor) load centers and on the Deadfront Trim for the NEMA 3R(outdoor) load centers.

Schneider Electric Canada

Attachment(s)
LC SCCR Bulletin Final Released 3-2014.pdf [2.29 MB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.