{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a cable operator be added to the Class 9422 Type T disconnect switches?
Issue:
Covert 9422 Type T to a cabled mechanism

Product Line:
Operating Mechanism and Disconnect Switches

Environment:
9422 Disconnect Switches

Resolution:
Non-cable operated mechanisms cannot be converted to cable operated and vice versa.
Available cable mechanisms can ONLY be installed in switches used with cable operators.
Note: This only applies for 30, 60 and 100 amp switches.

Switches compatible with cable operators.
Disconnect switch sizeFuse TypeFuse Clip Rating (A)Switch used with cable operators
250V600V
30 ANone--9422TCN30C
H, J, K, R30-9422TCF30C
60309422TCF33C
60 ANone--9422TDN60C
H, J, K, R60309422TDF60C
-609422TDF63C
100 ANone--9422TEN10C
H, J, K, R1001009422TEF10C

Cable operators to select based on desired cable length.
36 inch cable = 9422CFT30
48 inch cable = 9422CFT40
60 inch cable = 9422CFT50
120 inch cable = 9422CFT10

Schneider Electric Canada