{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the part numbers of the side plates covering the joint pack for 600A and 800A I-Line busway?
Issue:
What are the part numbers of the side plates (Tie channels) covering the joint pack for 600A and 800A I-Line busway?

Product Line:
I Line II Busway

Environment:
Maintenance

Cause:
Replacement

Resolution:
The covers are called tie channels.
The part number for the 600A tie channel is 45202-026-01 and it takes 2 per joint. The P/N for the Bag of Tie Channel Screws is 45132-001-55 / (1) required per joint.

The tie channel P/N for the 800A is 45216-108-01  and requires (2) per joint. The P/N for the Bag of Tie Channel Screws is 45132-051-50 / (1) required per joint



Schneider Electric Canada