{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are the 9001 KM11, 12, 13, 14, and 15 neon light modules a transformer type?
Issue:
Type of light module on 9001KM neon lights.

Product Line:
Push Buttons and Operator Interface

Environment:
Light Modules for Type K, SK and KX control units.

Resolution:
No, the neon units are a resistor style. The resistance value changes with each voltage rating, so the voltage at the lamp is always the same. This is why the same neon bulb can be used regardless of the voltage.

Schneider Electric Canada