{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What class of fuse is used in the QMB365W switch?
Issue:
Product design features

Product Line:
Heavy Duty Safety Switches

Resolution:
These switches accept class H or K fuses as standard. These are for use on systems with up to 10 kA available fault current. Alternative options include class R fuses (with class R fuse kit QMB4060R installed) and class J fuses (field relocate the fuse base assembly to alternate position marked in the enclosure). These are for use on systems with up to 200 kA available fault current.

NOTE: DO NOT USE RENEWABLE LINK FUSES IN SQUARE D SAFETY SWITCHES. The use of renewable link fuses may adversely affect user safety, impair reliability, and will void the warranty.

Schneider Electric Canada

Explore more
Product:
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: