{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the rubber gasket for 9001K and SK operators?
Issue:
Rubber gasket for 9001K and SK operators

Product Line:
Pushbutton and Operator Interface

Environment:
9001K and SK Operators

Resolution:
6509702001 is the black compensating gasket used with these operators. All operators come with 4 gaskets. These allow the operators to be used in various thickness enclosures with or without legend plates.

Schneider Electric Canada