{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is suffix S101 on an LC2D1201* S101?
Issue:
LC2D1201S101 information and replacement.

Product Line:
Tesys D line Contactors

Environment:
TeSys D Line Contactor

Resolution:
This was the standard reversing pre-TeSys D-Line contactor with A1 terminals wired together. Each contactor had 1 N.C. auxiliary contact. The mechanical interlock was standard design with no additional electrical interlocks. Coil voltage must be known to select proper replacement. Reversing power connections were also standard.

Replacement: Use standard LC2D12*
* = Voltage Code


Schneider Electric Canada