{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Does Schneider Electric have circuit breakers that can be used at 400 Hz?

Product Line:
Circuit Breakers

Resolution:
There are some Schneider Electric circuit breakers that may be used on a 400 Hz system, but rerating of the breaker will be required. Data Bulletin 0100DB0101, "Determining Current Carrying Capacity in Special Applications" shows the applicable circuit breakers, and explains how to rerate them. Here is the link to the bulletin:

0100DB0101

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: