{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the padlock attachment for a 9001 Type K or SK selector switch?
Issue:
Identify the padlock attachment for a 9001 Type K or SK selector switch

Product Line:
9001K, 9001SK - 30mm Push Buttons

Environment:
Pushbutton and Operator Interface

Resolution:
A 9001K7 or a 9001K107. The 9001K107 is spring loaded. They cannot be used with a gloved hand knob or the potentiometer operators.

Schneider Electric Canada