{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can I convert a TeSys overload relay to automatic reset from manual reset?
Issue:
Change from automatic reset to manual reset on a TeSys overload.

Product Line:
IEC Contactors and Starters

Environment:
TeSys Overload Relays

Resolution:
There is a small tab to the right of the current adjustment dial under the clear cover. Break this tab off to reveal a small switch that is used for this adjustment. There is an H and A to designate the settings; H for Hand and A for Automatic.


CTA-ID : 2008074

Schneider Electric Canada