{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a QO2150, QO2175, QO2200, or QO2225SL be used in a 300 or 400 A, QONQ load center?
Issue:
Can a QO2150, QO2175, QO2200 or QO2225SL be used in a QON load center?

Product Line:
QO

Resolution:
Yes, they can be used in QONQ, 300 and 400 A load centers (single phase only) for new installations.

NOTE: THESE BREAKERS CANNOT BE INSTALLED IN 3-PHASE LOAD CENTERS OR PANELBOARDS IN ANY CIRCUMSTANCE.

Schneider Electric Canada