{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do the 9001 SKRU push button units for the 9001 SKYP pendant stations include the contacts?
Issue:
Are the contacts included on the 9001SKRU pushbuttons when used on pendant stations 9001SKYP?

Product Line:
9001SKYP 30mm Pendant Station

Environment:
9001SKYP Push Button Units

Cause:
To determine if contact blocks need to be ordered along with the order.

Resolution:
The dual push buttons 9001SKRU** all include the contact blocks.

Schneider Electric Canada