{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is the breaker operating mechanism included with the 9422 flexible cable mechanisms?

Issue:
What is included with the 9422 Flexible cable mechanisms?

Product Line:
Operating Mechanisms and Disconnect Switches

Environment:
Class 9422 Operating mechanisms

Resolution:
Yes, unit includes breaker sadle, operating mechanism, cable mechanism. The operating handle assembly is also included with
the CGJ31 CGJ41 CGJ51 CGJ11 CFA31 CFA51 CFA11 CKA31 CKA51 CKA11 CLA31 CLA51 CLA11 units.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: