{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What does the Relay Accuracy Class mean for CT's?
Issue:
Accuracy Class rating on Current Transformers.

Product Line:
LV Transformers

Environment:
Applies to Current Transformers (CT's) by SquareD/Schneider Electric

Cause:
Many Current Transformers (CT's) are rated for both Relaying Accuracy and ANSI Metering Accuracy.  This FA is concerned with Relay Accuracy Class


Resolution:

A relaying accuracy class is designated by two symbols which effectively describe the capability of the transformer as follows:
C means the transformer ratio can be calculated, i.e. a window type current transformer with uniformly distributed windings. The C rating refers to a low-reactance design. The secondary terminal voltage rating is the voltage which the transformer will deliver to a standard burden at 20 times normal secondary current without exceeding 10% ratio error. Furthermore, the ratio error must be limited to 10% at any current from 1 to 20 times rated current at any lesser burden. For example, relay accuracy class C100 means that the ratio can be calculated and that the ratio error will not exceed 10% at any current if the burden does not exceed 1.0 ohms (1 ohm x 5 amperes X 20 times normal current = 100 volts). Note: Previous standards used the term 10L in place of C, such as 10L100, 10L400, etc. CSA Standard C13 used the term 10L in place of C.  For more information on instrument transformers, see the Instrument Transformer Catalog, document # 4210CT9701R6/01.


CTA-ID : 2009169

Schneider Electric Canada

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: