Search FAQs
What legend plates are used with the XACB pendant stations?
Issue:
Needs to know the legend plates are used with the XACB pendant stations.
Product Line:
Push Buttons and Operator Interface
Environment:
Pendant Stations
Resolution:
The standard 30mm X 40mm ZB2BY plastic legends that are used with the XACA pendant stations or the XB2 line of push buttons.
Needs to know the legend plates are used with the XACB pendant stations.
Product Line:
Push Buttons and Operator Interface
Environment:
Pendant Stations
Resolution:
The standard 30mm X 40mm ZB2BY plastic legends that are used with the XACA pendant stations or the XB2 line of push buttons.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: