Search FAQs
What Handles will 400A 9422 disconnects Accept?
Issue:
Looking for appropriate handle for the 9422TG1 and 9422TG2 Disconnect Switches
Product Line:
Operating Mechanisms, Disconnect Switches, and Door-Closing Mechanisms
Environment:
9422 Disconnect Switches
Resolution:
9422A7 - 12 in. handle for installation in enclosures rated 1, 3, 3R, 4 (sheet steel), and 12
9422A8 - 12 in. handle for installation in enclosures rated 4X (stainless steel)
9422A5 and 9422A6 are obsolete and was replaced by 9422A7 and 9422A8 respectively.
The Types A1 thru A4 and A9 and A10 are NOT designed to operate this disconnect switch.
Note: Caution should be used selecting this switch and handle assembly because commercial enclosure manufactures do not make a standard enclosure which will accept the Type TG switches. Special enclosures must be ordered from the enclosure manufactures.
Looking for appropriate handle for the 9422TG1 and 9422TG2 Disconnect Switches
Product Line:
Operating Mechanisms, Disconnect Switches, and Door-Closing Mechanisms
Environment:
9422 Disconnect Switches
Resolution:
9422A7 - 12 in. handle for installation in enclosures rated 1, 3, 3R, 4 (sheet steel), and 12
9422A8 - 12 in. handle for installation in enclosures rated 4X (stainless steel)
9422A5 and 9422A6 are obsolete and was replaced by 9422A7 and 9422A8 respectively.
The Types A1 thru A4 and A9 and A10 are NOT designed to operate this disconnect switch.
Note: Caution should be used selecting this switch and handle assembly because commercial enclosure manufactures do not make a standard enclosure which will accept the Type TG switches. Special enclosures must be ordered from the enclosure manufactures.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: