{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What circuit breaker enclosures will accept a FAL circuit breaker?
Issue:
What enclosures can be used with an FAL breaker?

Product Line:
Circuit Breaker Enlcosures=

Resolution:
The FAL frame circuit breaker can be mounted in the following enclosures:
1) FA100F (NEMA 1, flush mount applications)
2) FA100S (NEMA 1, surface mount applications.
3) FA100RB (NEMA 3R applications).
4) FA100DS (NEMA 1, 3, 3R, 4, 4X, 5, or 12 applications).
5) FA100A (NEMA 12K application)
6) FA100AWK (NEMA 1, 3R, 5, or 12 applications)
7) FA060X (60 A max, NEMA 7 application)
8) FA100X (NEMA 7 application)
9) FA060Y (60 A max, NEMA 9 application) or FA100Y (NEMA 9 application)

NOTE: The FAL circuit breaker can also be mounted in the KA225F (NEMA 1, flush mount applications), KA225S (NEMA 1, surface mount applications) or KA225RB (NEMA 3R applications). But these enclosures are all obsolete.

Schneider Electric Canada