{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Video: How is a GVAE11 mounted to a GV2ME__ manual starter?
Issue:
How can the GVAE11 be mounted on the front of a GV2 Starter?  

Product Line:
Tesys GV Manual Starter and Protectors
 
Environment:
GV2 and GV3 Manual Motor starters and protectors

Cause:
There does not appear to be a place to mount the device.

Resolution:
The GVAE11 is mounted to the front of the GV2ME starter. There is a plastic cover above the operator but below the line side lugs that is removed and disposed of. This reveals a cavity into which the GVAE11 is inserted.

Schneider Electric Canada

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.