{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why are rejection type fuses required to be used in the factory or field installed fuse clips of an Industrial Control Power Transformer?
Issue:
Fuses for Industrial Control Transformers

Product Line:
LV Transformers

Environment:
Applies to Industrial Control Transformers by SquareD/Schneider Electric

Cause:
Overcurrent protection (OCP) for CPTs

Resolution:

Rejection fuse clips have an AIR rating of 200,000 amps allowing end users to comply with UL 508 criteria for branch circuit status according to the NEC.

Schneider Electric Canada