{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the bonding strap used on 400A, 600A, and 800A NF panelboards?
Issue:
Bonding strap on NF Panel

Product Line:
Panelboards

Environment:
NF

Cause:
Replacement part

Resolution:
The NFBOND468 is the neutral bonding strap kit to be used when required on most 400 A, 600 A, and 800 A NF Panelboards.  However, the NFBONDGUTTER neutral bonding strap kit should be for NF Panelboards with Gutter Mounted Neutral Assemblies, including Condo Riser Neutral Assemblies.  These kits include lugs and required screws.  Please note that UL Service Entrance applications also require a main circuit breaker barrier kit.  Please consult the NF Merchandised Main Circuit Breaker interiors pages in Section 9 of the Digest for additional information.



Schneider Electric Canada