{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can an encapsulated wall mount transformer, type A, B or C, be mounted on its side or back?
Issue:
Mounting for encapsulated transformer with type A, B and C enclosure.

Product Line:
Transformers

Environment:
Resin Encapsulated Transformers

Resolution:
It can be mounted on its side or back, however it will no longer be rated Nema 3R. It will then be rated Nema 1. It should not be mounted with the wiring compartment facing upwards. This could result in the wiring compartment temperature exceediing the rating of the insulation system of the conductors contained therein.

Schneider Electric Canada