{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a Canadian QO (single phase) or CHOM main lug only load center be converted to a service entrance approved main breaker load center in the field?

Article available in these languages: Spanish

Issue:
Product Design Features

Product Line:
QO and CHOM Canadian load centers

Resolution:
No. The QO and CHOM main lugs ONLY load centers CANNOT be converted to a service entrance main breaker load center in the field. The Canadian code requires the main breaker, service entrance rated load centers to come bonded with the bonding screw factory installed. Also, the service entrance MB load centers contain a service barrier that prevents load branch wiring from exiting the mains area. In addition, per the code, the Canadian service entrance load centers require additional grounding points that a main lug load center does not contain.

NOTES:
1)A main lug load center could be converted to a main breaker subpanel using the appropriate QOM1 or QOM2 main breaker, depending on which MB the load center would use
2) A main breaker load center can be converted to a main lug load center for use as a subpanel ONLY by following the instructions on the label located on the service barrier; the label will state "CAUTION: This device is Field convertible to a NON SERVICE ENTRANCE Main Lugs or Main breaker load center when the box bonding screw is removed from the neutral AND this barrier is discarded."

Exceptions: The below catalog numbers are labeled 'Suitable for use as Service Equipment'
1) QO1L30S
2) QO2L70S (ONLY when used with one 2 pole breaker)
3) QO2L70RB (ONLY when used with one 2 pole breaker)

Schneider Electric Canada