Issue:
Using theGK2AF01 common mounting plate with GV2 and D-line contactor.
Product Line:
Contactors and Starters - IEC
Environment:
Tesys GV Manual Starter and Protectors
Resolution:
Yes it can. Do not use the GV2AF3 or GV2AF4 combination block when installing the GV2ME or GV2P and the D-line contactor on the GK2AF01 common mounting plate. The user will need to use either the GV1G02 flexible connector or their own flexible conductors.
Using theGK2AF01 common mounting plate with GV2 and D-line contactor.
Product Line:
Contactors and Starters - IEC
Environment:
Tesys GV Manual Starter and Protectors
Resolution:
Yes it can. Do not use the GV2AF3 or GV2AF4 combination block when installing the GV2ME or GV2P and the D-line contactor on the GK2AF01 common mounting plate. The user will need to use either the GV1G02 flexible connector or their own flexible conductors.
Released for:Schneider Electric Canada