{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the Nema type 3R/12, I-Line Panelboard Enclosures be Service Fed from Overhead or Top Fed?
Issue:
Is it possible for an I-Line Panelboard with Nema 3R/12 Enclosures be Top Fed or Bottom Fed?

Product Line:
Panelboard

Environment:
I-Line Panelboard

Resolution:
YES, Requires that the interior be rotated 180degrees and always check NEC before installation. Normally a Liquidtight or watertight hub is required when entering above live parts.

NOTE: There are instructions on the FAQ`s for converting a panel from bottom to top feed and vice versa. KEYWORD: TOP FEED, BOTTOM FEED


Schneider Electric Canada