{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the terminal lug data for ALL of the 600amp, US and Canada, Heavy Duty Safety Switches(for example, H266,CH226N, CH326NDS, H326DS, H366, H366R, HU366, HU366AWK and CHU366AWK )?
Issue:
Product Feature

Product Line:
Safety Switch

Cause:
Wire installation

Resolution:
The 600Amp Heavy Duty Safety Switches will accept as standard (2) #3/0 AWG through 500 KCMIL aluminum or copper wires per phase. The Lug conductor(or wire) temperature rating is 75 degrees C

NOTES:
1)
The only alternate lugs are compression lugs and they do NOT allow for any different wire size or quantity than what is shown above.
2) 90 degree wire can be used, BUT it MUST be sized per the 75 degree ampacity table in the National Electrical Code.

Schneider Electric Canada