{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the finish of QO and Homeline, NEMA 3R load center covers and boxes?
Issue:
Product Design features

Product Line:
QO Load centers

Resolution:
ALL the QO and Homeline, NEMA 3R (outdoor) load center covers and boxes are made of galvannealed sheet steel and painted (or finished) with an ANSI 49 gray paint, electrodeposited over clean, phosphatized galvannealed steel.

Schneider Electric Canada