{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the correct grease to use for Metal Enclosed Switchgear?
Issue:
Grease for HVL switchgear

Product Line:
Medium Voltage switchgear

Environment:
Maintenance

Resolution:
The correct grease to use for Metal Enclosed Switchgear and HVL gear  is Mobilgrease 28 red grease.  The part number for a 35 lb pail is 1615100950.  For a 12 oz tube of the same grease, the part number is 1615100950T.  
The old grease should be removed with contact cleaner before this new grease is applied. Good practice is not to mix two different greases.


 

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more