{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is replacement mechanical interlock available for LC2D1201?
Issue:
What is the mechanical interlock part number for LC2D1201?

Product Line:
IEC Contactors and Starters

Environment:
Tesys D accessories

Resolution:
Yes, order LA9D09978 or LA9D0902 which also includes (2) normally closed electrical interlocks.

NOTE: These have been obsoleted as well as the the contactor LC2D1201.
The new offer of contactors LC2D12** uses LAD9R1 OR LAD9R1V

**Coil Voltage

Schneider Electric Canada