{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can I use a drive on a Wye-Delta motor, instead of using a Wye-Delta open or closed transition starter?
Issue:
Identify the usage of a drive in a Wye-Delta configuration

Product Line:
ATV Drives

Environment:
Schneider Drives and Soft Starters

Resolution:
You can wire the motor in the Delta configuration, and let the drive do the soft-starting.
Size the drive according to the full load amps of the motor.

Schneider Electric Canada

Explore more
Product:
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: