Product Line:
Circuit Breakers
Resolution:
For breaker catalog numbers QOB2150VH, QOB3110VH, QOB3125VH, and QOB3150VH, the padlock attachment is built into the breaker. It consists of a small hasp with a loop that can be extended to allow a padlock to lock the breaker in the ON or OFF position. See the picture below.
Circuit Breakers
Resolution:
For breaker catalog numbers QOB2150VH, QOB3110VH, QOB3125VH, and QOB3150VH, the padlock attachment is built into the breaker. It consists of a small hasp with a loop that can be extended to allow a padlock to lock the breaker in the ON or OFF position. See the picture below.
- On the 2 pole breaker, the hasp is located in the body between the 2 poles
- On the 3 pole breakers, the hasp is located in the body between the 2nd and 3rd pole.
Released for:Schneider Electric Canada