Issue:
Is the 9999LB0 lug bar extender kit required for the Class 9065 Motor Logic Solid State Overload Relays?
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
Class 9065 Motor Logic solid-state overload relays (SSOLRs)
Resolution:
The lugbar kit is not needed, but sometimes it may be easier to install using the kit. For example; if retrofitting on existing starter and the motor leads are not long enough to pass through the CT windows the addition of the lug bar extender kit will resolve the issue without pulling new wires.
Is the 9999LB0 lug bar extender kit required for the Class 9065 Motor Logic Solid State Overload Relays?
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
Class 9065 Motor Logic solid-state overload relays (SSOLRs)
Resolution:
The lugbar kit is not needed, but sometimes it may be easier to install using the kit. For example; if retrofitting on existing starter and the motor leads are not long enough to pass through the CT windows the addition of the lug bar extender kit will resolve the issue without pulling new wires.