{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the replacement gasket for a 9001KY enclosure?
Issue:
Are gaskets for the 9001 enclosures replaceable?

Product Line:
Push Buttons and Operator Interface

Environment:
9001 KY Control Stations

Resolution:
For the 9001KY1 the part number is 3042630701.
2470D14X1 is the replacement gasket part number for the 9001KY2. However, this one is already obsolete.
The gasket for the 9001KY3 is not a field replaceable part.

Schneider Electric Canada