{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How do you calculate the maximum possible Available Fault Current at the secondary of a Transformer?

Issue:
Transformer Available Fault Current

Product Line
LV Transformers

Environment:
Applies to LV Transformers by SquareD/Schneider Electric

Cause:
Transformers are often connected to equipment that is rated for certain AIC, Average Interrupting Current, or Available Fault Current

Resolution:
Take the secondary full load current of the Transformer and divide it by the Transformer`s impedance. This is not necessary on Transformers below 15kVA, thus why UL does not require the impedance on the nameplate of Transformers below 15kVA. For example, a 75kVA Transformer with a 208Y/120 secondary and 5% impedance has a capacity of 208 amps on the secondary. The peak let through with an infinite source (worst case scenario) would have 208 / 0.05 = 4,160 amps of peak let through current (available fault current).

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.