{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are GV2ME** available with factory installed auxiliary contact blocks?
Issue
Can the GV2ME be ordered with auxiliary contact blocks pre-installed?

Product Line:
IEC Contactors and Starters

Environment:
Tesys GV Manual Starter and Protectors

Resolution:
France will build them this way but none of them are loaded to our system. Contact us with specific starter catalog number and we will verify with France. Once we have received confirmation, we`ll add it to our system and then an order can be placed. They are sold only in lots of 20.

Add suffix to GV2ME** as follows:

AE1TQ for GVAE1 block
AE11TQ for GVAE11 block
AN11TQ for GVN11 block

Schneider Electric Canada