{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What stress cones do we recommend for HVL/cc Switchgear?
Issue:
What stress cones do we recommend for HVL/cc Switchgear?

Product Line:
HVLcc

Environment:
Products sold in the United States.

Cause:
Assembly/Installation

Resolution:
HVL/cc terminations
Cables Standard Termination Height
24`` from floor to fuse support lug landing
24``from top plate to switch terminals
Top pullbox can increase distance to 40``
Stress cone (installed length)
RAYCHEM
5kV - 10.5``
15kV - 15``
25kV - 28``
35kV - 33``

3M COLD SHRINK
Stress cone (installed length)
5kV - 28kV -- 16.5``
34.5kV - 20.5``




Schneider Electric Canada