{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can there be top entry or top exit on N3R HVL/cc switchgear.

No, there cannot be TOP entry or top exit on N3R HVL/cc switchgear.

The options to resolve this are rear entry/exit with the use of optional rear extensions.

Also, Side entry or exit can be done with the addition of an incoming/outgoing terminal chamber.

The roof design of the N3R HVL/cc is not compatible with entering conduits. In addition, the conduits would enter directly over the switch terminals. The HVL/cc has reduced clearances and should not have any moisture dropping down on top of the switch.


CTA-ID : 2011855

Schneider Electric Canada