Search FAQs
What is the difference between IP 65 and IP 40 on selections of ZB4BL9334 dual pushbuttons?
Issue:
Need to know the difference between IP65 and IP40 rating
Product Line:
22 mm push buttons
Environment:
Products sold and used in the United States
Resolution:
IP 40 is protected against solid objects, but is not watertight, similar to NEMA 1, IP 65 is protected against dust and water jets, similar to NEMA 4.
(1st number )
Protection against contact and penetration of solid bodies
(2nd number )
Protection against the penetration of liquids.
4= protection against solid 0= not protected
6= Dust tight 5= protection against water jets
Need to know the difference between IP65 and IP40 rating
Product Line:
22 mm push buttons
Environment:
Products sold and used in the United States
Resolution:
IP 40 is protected against solid objects, but is not watertight, similar to NEMA 1, IP 65 is protected against dust and water jets, similar to NEMA 4.
(1st number )
Protection against contact and penetration of solid bodies
(2nd number )
Protection against the penetration of liquids.
4= protection against solid 0= not protected
6= Dust tight 5= protection against water jets