{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the dimensions of 25kV and 38kV HVL Switchgear?
Issue:
Dimensions of 25kV and 38kV HVL Switchgear

Product Line:
Medium voltage switchgear.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
The HVL Switchgear indoor and outdoor enclosures for 25.8kV, 29kV and 38kV have been updated and standardized and have revised dimensions as follows:

Indoor Outdoor
Switch Sections:

Depth 80.50`` (2045mm) 86.00`` (2185mm)

Height 120.00`` (3048mm) 127.00`` (3226mm)

Width 25kV 48.00`` (1220mm) 48.00`` (1220mm)

Width 38kV 60.00`` (1524mm) 60.00`` (1524mm)

Bus Transition Sections:

Width 26.00`` (660mm) 26.00`` (660mm)

Transformer Throats:

Width 24.00`` (610mm) 24.00`` (610mm)

All Meter Sections 25/38kV:

Width 60.00`` (1524mm) 60.00`` (1524mm)




Schneider Electric Canada