Search FAQs
How do you select an HVL/cc Main Tie Main with Automatic Transfer in the center of the lineup with MotorPact starter feeders on each side?
Issue:
Selection
Product Line:
INMVE - MV EQUIPMENT
Environment:
NEMA ICS 3, UL347, EEMAC G14-1, ANSI C19.7, IEC 60470, IEC 60529, IEC60694, IEC60129, IEC62271-102, IEC 62271-200, ANSI C37.20.7
Cause:
A complex application requires careful consideration of layout.
Resolution:
To select an HVL/cc Main Tie Main with Automatic Transfer in the center of the lineup with MotorPact starter feeders on each side:
Put the voltage-sensing VTs in an incoming auxiliary section and have the cables come in there rather than into the main switches.
Choose the load side connection of the mains to be To Motorpact
CTA-ID : 2011870
Selection
Product Line:
INMVE - MV EQUIPMENT
Environment:
NEMA ICS 3, UL347, EEMAC G14-1, ANSI C19.7, IEC 60470, IEC 60529, IEC60694, IEC60129, IEC62271-102, IEC 62271-200, ANSI C37.20.7
Cause:
A complex application requires careful consideration of layout.
Resolution:
To select an HVL/cc Main Tie Main with Automatic Transfer in the center of the lineup with MotorPact starter feeders on each side:
Put the voltage-sensing VTs in an incoming auxiliary section and have the cables come in there rather than into the main switches.
Choose the load side connection of the mains to be To Motorpact
CTA-ID : 2011870
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: