{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the replacement 48 volt direct current control coil for the LP*D25** or LP*D25**?
Issue:
What is the part number for the replacement 48 volt direct current control coil for the LP*D25** or LP*D25**?

Product Line:
D2 Series pre Tesys contactors only.

Environment:
Products sold in the United States.

Cause:
Product availability.

Resolution:
For standard coil (code ED) order LX4D4ED, for wide range coil (code EW) order LX4D4EW. Note these replacement coils are for D2 Series pre Tesys contactors only.

Schneider Electric Canada