{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do the U-Line starters have integrated suppression? What type of suppressor do we use?
Issue:
Identify if the U line has an integrated suppressor module.

Product Line:
TeSys U IEC Starters

Environment:
IEC Contactors and Starters

Resolution:
U-Line starters have integrated suppression. The LUC's A1 & A2 terminals are connected to a high power carbon resistor (used as current/voltage damper) connected in series with a varistor limiting electronic circuit control voltage available at its terminals. Capacitors (to cope with circuit current demand) are connected in parallel with the varistor. The coil itself has a diode + Zener diode to limit the voltage on de-energization to around 24v. No additional suppression is required.


Schneider Electric Canada