Issue:
Viewing window availability on Legacy breakers
Product Line:
Legacy Breakers
Resolution:
This option is called Visi-blade, which has the individual viewing windows for each contact. Add "V" at end of breaker part number for the Visi-blade feature on these breaker types.
Viewing window availability on Legacy breakers
Product Line:
Legacy Breakers
Resolution:
This option is called Visi-blade, which has the individual viewing windows for each contact. Add "V" at end of breaker part number for the Visi-blade feature on these breaker types.
[3] FH circuit breaker is not UL Listed.
[4] Not available on 1P FA/FH circuit breakers.
The FA and FH breakers are now obsolete and this feature is not available on any Powerpact or Masterpact breaker frame. [4] Not available on 1P FA/FH circuit breakers.