Search FAQs
Are the on-delay and off-delay Electronic Serial Timer Modules available for the Tesys D-Line contactors?
Issue:
What is the part number for the electronic timer modules used for the Tesys D Contactors?
Product Line:
IEC Contactors and Starters
Environment:
Tesys D Contactors
Resolution:
The on Delay electronic timer modules are available. Used with LC1D09-65A @24-250Vac and LC1D80–D150 @100-250Vac
0.1–2 s LA4DT0U
1.5–30 s LA4DT2U
25–500 s LA4DT4U
Suggest the use of a separate mounted electronic timer such as the 9050JCK type in place of the off-delay module.
What is the part number for the electronic timer modules used for the Tesys D Contactors?
Product Line:
IEC Contactors and Starters
Environment:
Tesys D Contactors
Resolution:
The on Delay electronic timer modules are available. Used with LC1D09-65A @24-250Vac and LC1D80–D150 @100-250Vac
0.1–2 s LA4DT0U
1.5–30 s LA4DT2U
25–500 s LA4DT4U
Suggest the use of a separate mounted electronic timer such as the 9050JCK type in place of the off-delay module.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: