undefined undefined
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the external toggle handle for a Class 2510 FW or KW available as a repair part?
Issue:
Is the external toggle handle for a Class 2510 FW or KW available as a repair part?

Product Line:
2510 type F manual starter or type K manual switch

Environment:
Products sold and used in the United States

Cause:
External switch for the 2510 type FW or 2510 type KW needs to be replaced

Resolution:
Yes, order Class 9998 HW1. Kit includes On/Off button, shaft, ``O`` Ring, and roll pin.

Schneider Electric Canada