{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What fuse type is required for the 8538SB*12/13/22/23/62/65 combination starter?

Issue:
What class of fuses are used with NEMA Size 0 combination starters?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
8538 type S combination starters

Resolution:
This device is configured from the factory to accept Class H, J, K or R fuse types. However, this device is not supplied with Class R rejection pins. If Class J type (applications above 250 volt) fuses are used it will require re-positioning of the fuse base.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: